Energy chains - igus Blog - Page 3 Energy chains - igus Blog - Page 3

Tag: Energy chains

Can I also get a coloured energy chain?

Phillip Hagedorn | 3. July 2019

Yes. The basic igus energy chains are always black. e-chains in any colour shown in the colour selection chart are subject to a percentage-based colour surcharge. Any other colours that are not shown in the chart are individually calculated depending on the part and quantity, insofar as this is technically possible. Vote Up +0 Vote […]

Read more...

How long is the service life of an e-chain system?

Marco Thull | 1. July 2019

The service life of any energy chain system can be determined online with the help of the service life calculator. Vote Up +0 Vote Down -0You already voted!

Read more...

How do I find the right energy supply system?

Marco Thull | 1. July 2019

With the help of the e-ketten Expert, you can configure the right energy supply system online and then directly order it online together with the appropriate cables, which are supplied ready-to-connect. The Expert (using AI) calculates the optimum interior separation layout. However, a technical sales consultant is always available, of course, to help you design […]

Read more...

What must I bear in mind if I use hydraulic hoses?

Marco Thull | 1. July 2019

In e-ketten, all media can be guided easily and safely – including hydraulic and water hoses. Ideally, they are laid individually and are allowed 20% extra installation space. Their behaviour under pressure is to be considered when a choice is made, also when the strain relief system and interior separation layout are selected. For such […]

Read more...

How can I reduce the number of cable drums?

Marco Thull | 1. July 2019

All media can be supplied safely and reliably with only one energy chain system. Vote Up +0 Vote Down -0You already voted!

Read more...