Connectors - igus Blog Connectors - igus Blog

Tag: Connectors

What does the IP protection class say about a connector?

Beke Nieszytka | 8. July 2019

IP stands for International Protection or Ingress Protection. The IP, in combination with the following codes, gives precise information about the external influences against which a product is protected. The national and international standards DIN EN 60529 and ISO 20653 define these combinations and the type of protection in the different IP classes. Possible specifications […]

Read more...