cold - igus Blog cold - igus Blog

Tag: cold

Can igus energy chains be used in the refrigeration sector?

Marco Thull | 3. July 2019

Yes, all igus energy chain materials can be used for continuous use down to -40°C. Vote Up +1 Vote Down -0You already voted!

Read more...

Will the e-chain function even during cold weather/in combination with snow and ice?

Marco Thull | 1. July 2019

Our energy chains are very robust and even withstand extremely low temperatures below freezing point. Every one of our energy chains is tested in a cold chamber at -40 degrees Celsius in our test laboratory as well as in an outdoor test facility under real conditions. In the event of special requirements, our energy chains […]

Read more...