With the aid of 3D printing, injection moulds can be manufactured at up to 80% lower costs. As a result, 3D-printed moulds are particularly interesting for small batches and samples, and can be commissioned for a quantity of 1 or more. The complete iglidur range of 50 materials is available for the maintenance-free plastic plain […]
Basically, a 3D printer works much like a well-known 2D printer that applies ink to a paper by means of a jet or laser. The 3D printing is an additive process in which material is gradually added layer by layer to create a three-dimensional model. There are several methods in 3D printing that work slightly […]
Depending on the alignment of the component during printing, different results may occur for the surface. Depending on the printing process, this more or less influences the quality of the finished component. Therefore attention should be paid to the alignment while printing, whether there are certain functional areas in the component, where a smoother surface […]
Depending on the requirements of the finished component, 3D printing also requires a certain amount of reworking of the printed parts. For example, support structures or masses have to be removed manually. Likewise, the parts are subjected to various methods of blasting or vibratory finishing as required. Manual sanding may also be required to get […]
The accuracy of a 3D printing part depends on the respective method and the quality of the printer. The filament used and the quality of the CAD data also play a role here. Basic information on tolerances in 3D printing Compared to injection moulding or machining processes, the possible deviations are greater in 3D printing. […]