Why do the plain bearings not need any lubrication? - igus Blog Why do the plain bearings not need any lubrication? - igus Blog

Why do the plain bearings not need any lubrication?

Lars Butenschön | 2. July 2019

Why do the plain bearings not need any lubrication?

You are here:

Due to the special make-up of the iglidur materials, which are usually composed of a thermoplastic matrix, fibre reinforcements and so-called solid lubricants. The good wear and friction properties of the matrix or base material are additionally enhanced by the solid lubricants. During operation, there are always enough particles of solid lubricant on the surface of the bearing. Additional lubrication from the outside with grease or oil is usually not necessary or useful. Video regarding the question

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Plain bearings

Newsletter:

Choose a topic now