Ready-to-Connect - igus Blog - Page 2 Ready-to-Connect - igus Blog - Page 2

Category: Ready-to-Connect

What does IP54 mean?

Beke Nieszytka | 8. July 2019

A product with IP54 degree of protection has complete contact protection. In addition, it is protected against splashes of water. Vote Up +0 Vote Down -0You already voted!

Read more...

How are harnessed igus cables tested?

Beke Nieszytka | 8. July 2019

After harnessing, all cables pass through our test field. Depending on the specification, various tests can be carried out here. igus works on 10 test fieldswith 3,000 different test adapters. The following tests among others are performed: Digital logic tests High-voltage tests Network tests Attenuation tests Upon request: Customised tests After each test, the associated […]

Read more...

What are the connection types available?

Beke Nieszytka | 8. July 2019

The following connection types are available: Screw connection Axial screw connection Crimp connection Cage clamp connection Solder connection Wrap post connection Insulation displacement connection Press-fit technology Fibre optic connection Vote Up +1 Vote Down -0You already voted!

Read more...

Can harnessed cables also be individually labelled?

Beke Nieszytka | 8. July 2019

Yes, harnessed cables can be customised.All harnessed cables are marked with a label on each side. In addition, many cable inscriptions can be stamped, embossed, engraved, lasered or printed with industrial grade ink. Vote Up +1 Vote Down -0You already voted!

Read more...

Why is the right filling of an energy chain so important?

Beke Nieszytka | 8. July 2019

The arrangement of cables and hoses is very important to the service life of the e-chain system. The use of separators and shelves significantly improves the service life of cables and hoses. The arrangement of the cables themselves also plays a role and has a positive/negative effect, among other things, on the signal transmission, abrasion […]

Read more...