Yes. Regarding shafts for iglidur plain bearings, we recommend a roughness of 0.2 µm to 0.4 µm. A low degree of roughness can cause stick-slip effects or very fine nicks in the plastic, which can occur as a consequence of high adhesion forces. You can read more about “The right surface finish for shafts” in ourblog article. Vote […]
If you know the composition of the cleaning agent or generally of the medium, you can choose the chemical-resistance of our materials in our iglidur Expert system, for example, and thus find the appropriate iglidur product. The iglidur materials of the “H family” (iglidur H1, H370 etc.) and iglidur X are regarded as especially resistant to chemicals. Vote Up +1 […]
Yes, we supply FDA-compliant slewing rings. They have iglidur A180 plain bearings and stainless-steel rings. Vote Up +0 Vote Down -0You already voted!
Jammed plain bearings can have different causes such as housing holes with insufficient tolerance, as a result of which compression of the bearings and thus reduction of the inner diameter occurs. Another reason that is often observed is an insufficiently deburred hole. If the bearing is press-fitted carelessly, even small pieces of material residue can […]
In view of the more than 60 different iglidur materials and innumerable plastic or metal plain bearings of other suppliers, it can be difficult to choose the right plain bearing that you need. We are very familiar with the problems involved in choosing the right product for new bearing applications. For this reason, we have developed […]