drylin® linear technology - igus Blog - Page 5 drylin® linear technology - igus Blog - Page 5

Category: drylin® linear technology

Can I set different acceleration profiles in the D3 DC motor control?

Michael Hornung | 8. July 2019

That works. And yes, right on the housing. And yes it’s really easy. Because, the D3 DC motor control offers a selection between 5 different acceleration settings (also acceleration profiles or ramps).  And the selection is carried out like this. Tip For those who want to know and read more about the operation of the […]

Read more...

How do I know the IP address of a D1 motor control?

Michael Hornung | 8. July 2019

A hallmark of a modern motor control system for stepper and DC motors is the ease of use. But before the simple operation is the easy connection. And that’s especially easy with the dryve D1 motor control. Without any software just enter the IP of the D1 in the browser of your choice and off […]

Read more...

How do I connect a DC motor control with a linear axis?

Michael Hornung | 8. July 2019

The most important steps of connecting a D3 DC motor control to a linear module or a linear axis to a DC motor can be found here. And regardless of whether the module is operated with a lead screw or a toothed belt.   Tip For those of you who want to know and read […]

Read more...

Do not take it too seriously. The D3 DC motor control in alternative use.

Michael Hornung | 8. July 2019

Even unusual applications can be implemented with the D3 DC motor control. Everything is possible, because the operation is very simple. The control system on the housing itself enables mobile use. You can see a few ideas here. … and you can buy the DC motor control here. No minimum quantity, and delivered in 24 […]

Read more...

The assembly advantage of a split linear plain bearing

Michael Hornung | 5. July 2019

As an alternative to lubricated ball bushings, there is the clean self-lubricating alternative of a linear plain bearing adapter. The two cylindrical types have identical installation heights and can be installed in any linear housing. The assembly in the housing is also identical for both bearings. With a split housing, the replacement of the bearing […]

Read more...