In addition to the inductive proximity switches, mechanical proximity switches can also be connected to the D3 DC motor control. You will find everything about the installation here. Tip For those who want to know and read more about the operation of the D3 DC motor controller, see here for the complete manual. Vote Up […]
The dryve D1 is THE motor control for stepper motors and DC motors. An explanatory video> will show you which power supplies can be used for the operation of the D1. The complete manual for the dryve D1 can be downloaded here. Vote Up +0 Vote Down -0You already voted!
They are still available, good simple things that are also cost-effective. The example of a motor control for DC motors means that it is easy to connect and control right on the housing important things such as direction or speed. You can see here how that will look like in everyday life. Tip […]
That works. And yes, right on the housing. And yes it’s really easy. Because, the D3 DC motor control offers a selection between 5 different acceleration settings (also acceleration profiles or ramps). And the selection is carried out like this. Tip For those who want to know and read more about the operation of the […]
A hallmark of a modern motor control system for stepper and DC motors is the ease of use. But before the simple operation is the easy connection. And that’s especially easy with the dryve D1 motor control. Without any software just enter the IP of the D1 in the browser of your choice and off […]