drylin® linear technology - igus Blog drylin® linear technology - igus Blog

Category: drylin® linear technology

What all can I adjust directly on the D3 DC motor control?

Michael Hornung | 8. July 2019

You do not need a laptop, pad or smart phone to operate the dryve D3 DC motor control. The most important functions can be found directly on the housing and this makes the motor control very mobile and very easy to operate. Convince yourself. Vote Up +0 Vote Down -1You already voted!

Read more...

How do I connect a mechanical proximity switch to a D3 DC motor control?

Michael Hornung | 8. July 2019

In addition to the inductive proximity switches, mechanical proximity switches can also be connected to the D3 DC motor control. You will find everything about the installation here. Tip For those who want to know and read more about the operation of the D3 DC motor controller, see here for the complete manual. Vote Up […]

Read more...

Which power supplies can be used with the D1 motor control?

Michael Hornung | 8. July 2019

The dryve D1 is THE motor control for stepper motors and DC motors. An explanatory video> will show you which power supplies can be used for the operation of the D1. The complete manual for the dryve D1 can be downloaded here. Vote Up +0 Vote Down -0You already voted!

Read more...

Where do I use a motor control for DC motors?

Michael Hornung | 8. July 2019

They are still available, good simple things that are also cost-effective. The example of a motor control for DC motors means that it is easy to connect and control right on the housing important things such as direction or speed.   You can see here how that will look like in everyday life.   Tip […]

Read more...

Can I set different acceleration profiles in the D3 DC motor control?

Michael Hornung | 8. July 2019

That works. And yes, right on the housing. And yes it’s really easy. Because, the D3 DC motor control offers a selection between 5 different acceleration settings (also acceleration profiles or ramps).  And the selection is carried out like this. Tip For those who want to know and read more about the operation of the […]

Read more...