Interconnection of the hall sensor (revised and posted on 15/03/12) - igus Blog Interconnection of the hall sensor (revised and posted on 15/03/12) - igus Blog

Interconnection of the hall sensor (revised and posted on 15/03/12)

Martin Raak | 13. September 2012

The hall sensor Honeywell SS443A has an open collector output. This is intended for connection to a TTL/CMOS circuit – the 10kΩ pull-up resistor is already on the board. In this case no further circuitry is necessary.

In our test facilities, we like to apply the output to a 24V controller (e.g. PLC). This can be for example implemented by the following circuit with optocoupler module. The components have to be adapted to the respective load accordingly:

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!