How do iglidur plain bearings reduce noise in motor vehicles (Buzz, Squeak and Rattle)?
Julio Pauli | 2. October 2019

What is Buzz, Squeak and Rattle (BSR)?
BSR are all noises that are produced by components and assemblies in the motor vehicle. BSR testing, also called a noise and rattle test, is an acoustic method from the automotive industry and is used to measure the volume of these noises. A realistic situation with corresponding vibrations is simulated and the volume of the noise is then measured. The technical challenge for the vehicle and component engineers is to identify the ‘noisy’ components and replace them with a quieter solution wherever possible.
The expectations of the OEMs in this context are increasing continually. In the case of alternative drives such as the hybrid or electric motor, the noise of the drive is reduced, as a result of which noises inside the vehicle are masked to a much lesser extent by a loud combustion engine. At the same time, it is becoming quieter and quieter inside motor vehicles.

How do iglidur plain bearings reduce noise?
Noises always arise where components interact with each other, in other words where friction occurs. With the tribologically optimised high-performance polymers from igus, you achieve an especially low coefficient of friction and therefore a quiet application. Whether in vehicle seats, hinges or actuators, the variety of applications for our iglidur plain bearings inside vehicles is great.
Polymer is characterised by the fact that, unlike metal, it has a damping effect. In applications involving severe vibrational stress, a polymer bearing solution helps to reduce noise inside motor vehicles. The range of materials developed by igus includes materials that have especially good damping properties.
Further reasons for using iglidur in motor vehicles can be found here: https://www.igus.eu/info/5-reasons-for-the-use-of-iglidur-plain-bearings-in-automobiles?L=en
PS: whether plain bearings, spherical bearings, linear bearings, special sliders, gear or individually customised geometry, the iglidur® Designer leaves nothing to be desired.
Request your part now and receive a quote by tonight.