First self-programmed pick & place applications with our new software - igus Blog First self-programmed pick & place applications with our new software - igus Blog

First self-programmed pick & place applications with our new software

Martin Raak | 24. September 2012

At the MOTEK 2012 in Stuttgart, we are presenting a new robolink software with which the customer can program simple applications with our robolink articulated arms (see picture: screenshot of the programming interface):

 

 The program was developed by Professor Behnke of the Institute of Computer Science, University of Bonn. His team is the current world champion in robocup “teen size league” as well as in “robocup at home.” The interface is inspired by the programming interface of the soccer robot and is very intuitive to use. I myself had no definite idea about programming but was able to program this process within a few minutes with the software (see film). Alright, the film is not madly spectacular, but for us it is a big step in making the robolink joint kit for simple applications easy to use. The following are required as control components (not supplied by igus®): stepper motor controls of NANOTEC SMCI47-S2 (one per motor or per degree of freedom) and a simple little control board as master controller (CRUMB 2560 costs about € 45,00). We’ll be presenting more details on the software at Motek in Stuttgart.

 Video

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!