Energy chain? - igus Blog Energy chain? - igus Blog

Energy chain?

Marco Thull | 14. November 2019

Polymer energy chains with cables guided in a trough

Generic terms

The term e-chain is closely related to the terms drag chain, energy chain and energy supply system or energy guiding chain or even cable guidance systems.

The e-chain describes a product which safely carries cables or even hoses, over a certain distance. They ensure the dependable supply of energy, data and signals while in constant motion. They were developed to guide and protect. igus® has been developing, producing and testing polymer energy chains since 1971. There are energy chains made of plastic or metal (steel or aluminium) and of a combination of both materials, the so-called hybrid chains.

Types

There are different types and versions of energy chains to meet different requirements. For example, there are completely enclosed versions that withstand external influences such as dirt or swarf and still guarantee the function of the machine. Variants specifically designed for multiple directions of movement, such as on robots, are also common, as are special materials, that prevent static charges or are suitable for food processing areas (FDA).

Variety of energy supply systems

Energy chains are described as one of the most modular possibilities of energy supply systems. There are other possibilities, such as festooning (cable loops), which are often seen on cranes in ports and so on. With festoonings, cables “hang” freely and loosely on cranes in wind and weather. There are also motor cable drums,, busbar systems or inductive transmission. Here, for example, it is rather difficult to carry air or liquids, even light waves, whereas in an energy chain it can simply be carried along with data and signals.

The term e-chain is closely related to the terms drag chain, energy chain and energy supply system or energy guiding chain or even cable guidance systems.

The latest generations of energy chains focus especially on very easy assembly and filling. In addition, noise reduction, increased stability and lower weight are also important.

Saving installation time and costs: An energy chain that can be opened and closed in seconds without tools plays out its advantages here.

Reduction of the noise level of the entire plant/machine: Smooth operating energy supply systems are often the first choice here.

Small installation spaces and dimensions of the machines/plant: Smaller energy supply systems with the same or higher stability than their predecessors demonstrate their advantages here.

Higher dynamics of machines/plant: Reduced moving masses due to lighter energy supply systems are a topic here.

The latest generation of energy supply systems should always be considered for new and innovative machines and systems.

E4Q from igus® – one of the latest generations of e-chains

Order energy chains directly or request samples here

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!