Comparison of plain bearing materials: bronze bushings and other alloys - igus Blog Comparison of plain bearing materials: bronze bushings and other alloys - igus Blog

Comparison of plain bearing materials: bronze bushings and other alloys

Lars Butenschön | 14. May 2021

Bronze bushings, like many other purely metallic bushings, are based on a so-called alloy. In this process, metallic “mixtures” are created by melting together different types of metal, which in turn have different specifications. A direct comparison of these different alloys with the no less numerous different polymer compounds, which are common in polymer bearings, is accordingly difficult. Nevertheless, this blog post should help to better distinguish between the two technologies and facilitate the decision for or against one or the other.

The operating principle of bronze bushings and other solid bearings

Bronze bushings belong to the group of solid bushings or solid bearings. They consist of a single material or alloy. Similar to the solid plastic bushings, there is no sliding or supporting layer here. What all metal alloys have in common is their limited suitability as sliding materials. In conjunction with metallic shafts, it is important for all solid bushings that are regularly subjected to stress. To provide cooling and reduce friction by supplying lubricants.

The problem: without externally supplied lubrication, metal solid bearings are at best suitable only for so-called emergency operations. In practice, one speaks of emergency operating features when the bushing can still continue operation long enough in the event of an interruption in the power supply to allow the unit to be promptly switched off. An example of these emergency running functions are pumps whose bearings are often designed to be lubricated and cooled by the medium being pumped.

This need for permanent lubrication results in corresponding design requirements for the components. That is why bronze bushings and other solid bearings have the so-called lubrication grooves. These are milled or turned channels running along the inner and/or outer diameter, through which the lubricant can be distributed to the bearing point. However, the production of these bushings is quite expensive, especially for larger quantities, as the lubrication grooves have to be made individually on appropriate milling machines or lathes.

Bronze bushing with lubrication holes
Bronze bushing with lubrication holes (Source: igus GmbH)
Technical specifications of bronze bushings and solid bearings

The possible combinations of the different metals are manifold, which is not only due to the basic metals available for selection and their combinations, but also because these metals can in turn be used in different proportions. In view of this diversity and without metallurgical details, a detailed comparison is beyond the scope of this blog. However, here is a rough overview of some common alloys and their specifications:

CuSn7Zn4Pb7-Bronze DIN EN 1982 (CC493K)

  • Most common and cost-effective red bronze (gunmetal) alloy for plain bearings.
  • Good emergency operating specifications as well as sufficient wear resistance under medium loads.
  • Also for unhardened shafts and light edge pressure.

CuSn12-C

  • Tough bearing material with good sliding properties and good wear resistance
  • Especially for high surface pressures and simultaneously occurring impacts

CuSn8

  • Very good sliding properties, high wear resistance and good heat resistance.
  • Suitable for high speeds and high loads if sufficiently lubricated and with hardened shafts
  • Particularly suitable for thin-walled bushings

There are many other variants that are suitable for a wide range of applications depending on their specifications.

Bronze bushings compared to plastic bushings

Broken down purely to the individual technical values, the two material groups are difficult to compare meaningfully. Like most metallic bushings, bushings made of bronze or similar alloys offer higher mechanical strength values and – at least when lubricated – better pv values. The consideration should therefore take place above all with regard to the framework conditions. Polymer bushings, for example, often offer cost savings due to the possible elimination of lubrication and more cost-effective production. In addition, depending on the polymer compound, the pure material costs can also be significantly more cost-effective. The elimination of the need for externally supplied lubrication also results in further advantages in terms of dependability and maintenance of the bushings. Furthermore, weight savings due to the lighter material are also not insignificant, depending on the application.

Advantages and disadvantages of bronze bushings and solid bearings versus plastic bushings

Benefits

  • Higher strength values
  • Better pv values (if lubricated)
  • Higher surface speed possible (if lubricated)

Disadvantages

  • Need to be lubricated
  • More complex and therefore more expensive to manufacture (lubrication grooves or holes)
  • Increased weight
  • Susceptible to corrosion (depending on alloy)
  • Not RoHS compliant (depending on alloy)
Brass bearing with wear marks on the inner diameter
Brass bearing with wear marks on the inner diameter (Source: igus GmbH)
Looking for the optimum plain bearing? We would be glad to assist you!

In every plain bearing application, these advantages and disadvantages have to be weighed up against each other. However, not all of these aspects play a role in every application. In addition to bronze bushings, gunmetal bushings or other solid bearings, there are other bearing types that in turn have other strengths and weaknesses.

The different types of plain bearings are suitable for different applications in different specifications. Often there is an overlap of applications – but not infrequently there are major differences in service life and performance.

Our application specialists will be happy to advise you and design your bearing point together with you. We will determine the plain bushing with the best ratio of service life, costs and performance for you – by telephone, via digital visit or at your site. Free of charge and without obligation. Everything from one source.

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!