Worum geht es? Beim Abbau sowie bei der anschließenden Lagerung von Bauxit, einemSedimentgestein zur Aluminiumoxidproduktion, bildet sich eine MengeStaub, der vor allem für die beweglichen Maschinenteile derFördereinheiten eine große Herausforderung darstellt. Um den Einsatz von Energieketten noch sicherer und gleichzeitig auch bequemer zu machen, kommt die Zustandsüberwachung (Condition Monitoring) EC.P zum Einsatz. Was ein EC.P […]
Nowadays, the field of condition monitoring is all-encompassing. There are hardly any things or places that are not permanently monitored. Some people already associate the concept of monitoring with negative aspects from this point on. However, in the field of energy supply, condition monitoring should be a positive, useful, helpful and safe monitoring. The ultimate […]
News from the smart plastics test laboratory On 11.08.2020 with very warm temperatures (+35°C) outside, BTG and us as well as the EC. PP (positioning system for long travels). entered the hot phase. The system presented in spring 2020 now takes the next major step in readiness towards high volume production. The aim is to […]
Offshore – where service work costs millions: is that really necessary? Energy supply at drilling rigs, construction machines and shore power applications – cold, wet, dirty and heavy. Real stress for thick cables, hard hoses, but also for sensitive bus and data cables. Too much stress leads to breakages – which usually cost a lot […]
Offshore – where service work costs millions: is that really necessary? Energy supply at drilling rigs, construction machines and shore power applications – cold, wet, dirty and heavy. Real stress for thick cables and hard hoses, but also for sensitive bus and data cables. Too much stress leads to breakages – which usually cost a […]