Ball bearings have become indispensable in mechanical engineering. There are various ball bearing designs for which mass and technical composition of the components depend on the specifications of the industrial application. The following list shows the most frequently used ball bearings and where they are used: Deep groove ball bearings according to DIN 625: This […]
The material for rolling bearing ball bearing balls varies widely and is always primarily focused on the ring materials. This ensures that the interplay of cage, inner ring, and outer ring in the system is harmonised. This is especially important when the application involves heating or cooling the bearings. It is important that ball bearing […]
Choosing the right material for ball bearings is not always easy. A short summary, when I use a particular ball bearing. Limits of metallic ball bearings Metallic ball bearings are mainly used in most classic mechanical engineering applications. They rank number 1 in terms of global sales volumes and are suitable for a large number […]