Martin Raak - igus Blog - Page 29 Martin Raak - igus Blog - Page 29

igus® robolink® with pneumatic gripper

Martin Raak | 7. February 2012

We build demonstration plants time and again for our own trade shows and of course for our igus® subsidiaries all over the world. Such systems are then shown, for example at the Hannover Messe or Motek, as well as in many smaller or the so-called house shows of customers.For some time we’ve been equipping our […]

Read more...

Tensile strength test report of robolink® wires

Martin Raak | 26. January 2012

robolink® wires were tested for tensile strength on the ZWICK tractor (nominal tensile strength > 3600 N).The nipple connection was fixed with different adhesives (see installation instructions for the wires). The experiments were carried out at room temperature and at 80°C.          Wire with brass nipples  Section of the mounted nipple Test […]

Read more...

igus® 4 DOF arm with drive unit in use

Martin Raak | 9. January 2012

Polytechnico di Torino in Italy uses a robolink® 4-axis arm with drive unit and angle sensors. Movement with voice control Vote Up +0 Vote Down -0You already voted!

Read more...

Robot “Flash” in London Science Museum

Martin Raak | 22. December 2011

Wroclaw University of Technology (Poland) has equipped its robot “Flash” now with the latest version of robolink® arms. Whereas only one arm was mounted in the first version, now both arms are used. The robot was unveiled in this version for the first time at the Robotville Festival in the London Science Museum in early […]

Read more...

robolink® articulated arm at ECHORD project

Martin Raak | 15. December 2011

Fraunhofer Institute IFF, Magdeburg, takes part with a robolink® articulated arm in the ECHORD project The IFF examines kinematic models with this special construction of a 4-axle articulated arm.The structure with 3 joints in a series, wherein the rotational axes of the two first joints were shut down, is a special design.The drive system is […]

Read more...