Underwater use presents some special challenges for machines in general and for bearing arrangements in particular. The main problem is obvious. The water – but also other liquids – affects the bearing points in various ways. In this blog post you will find out what these are and what you need to bear in mind […]
Lubrication grooves perform an important task in metallic bearings. The lubricant reaches the bearing point between the bearing and the shaft directly through them. The lubricant protects the shaft and bearing against dirt and moisture and ensures low coefficients of friction. Disadvantages: On the one hand, a bearing with a lubrication groove is quite complex […]
Bearing damage can often be traced back to an insufficient press fit. In addition to inadequate lubrication or incorrect design, bearing bushings that are insufficiently located in the bearing position are among the most frequent causes of premature failures. There are many reasons for insufficient press fit. But did you know that anti-corrosion agents are […]
If you want to always be able to install your bushings, especially plain bushings, without frustration or damage, you should follow a few basic tips. This post will list these tips and provide an explanation for each. Before press-fitting the bushing: Pay attention to tolerances and fit-related oversizing Plain bushings must be press-fitted because they […]
Where are plain bearings used? And when should you use metal plain bearings, and when plastic ones? It is not easy to give clear answers to these questions. The market is large and complex, and new products keep getting launched, shifting the limits of applicability and offering new advantages. But I will give you a […]