Lars Butenschön - igus Blog - Page 4 Lars Butenschön - igus Blog - Page 4

How are plain bearings constructed?

Lars Butenschön | 4. March 2022

One of the main features of plain bearings – compared to ball or rolling bearings – is their significantly less complex design. But is that really the case? In fact, different types of plain bearings differ significantly in how they are constructed and how they work. In this blog post, you will learn all about […]

Read more...

Gluing bushings – this is how it works

Lars Butenschön | 25. February 2022

Bushings are usually pressed or clamped into the housing hole. In this way they hold securely in the hole and do not rotate unintentionally. But what if this is not possible due to manufacturing tolerances? Another not so rare case: The bushing should even rotate. Even if it is not part of the standard repertoire […]

Read more...

Plain bearings for high speeds? Where are the limits?

Lars Butenschön | 10. December 2021

“Plain bearings are particularly suitable for high loads at low speeds.” This, or something similar, is what many technical books, guides, and also advertising texts say. There are two things about this statement that are not particularly helpful in practice. This blog post will analyse this statement and the conditions under which certain types of […]

Read more...

How high temperatures affect plastic plain bearings

Lars Butenschön | 26. November 2021

“What temperatures can they handle?” is certainly one of the most frequent questions I have been asked at trade fairs. (Remember trade fairs? With handshakes and everything?) The only questions more common were “How long does it last?” and of course “Do you have a business card?”. But back to the subject of high temperatures […]

Read more...

Correctly select piston rings

Lars Butenschön | 12. November 2021

As with most machine components, the devil is in the details when it comes to choosing the right piston ring. For one thing, it depends on details such as slot design and fixing groove depth and width. For another, the material plays an important role and affects installation tolerances in its turn. You can find […]

Read more...