Alexander Muzicenko - igus Blog Alexander Muzicenko - igus Blog

Do polymer plain bearings in bicycles have to be lubricated?

Alexander Muzicenko | 15. September 2020

Polymer bearings have already been used in bicycles for many years and are gaining more and more popularity – whether in pedals, frame bearings or gears. iglidur® materials offer more advantages such as: weight reduction, corrosion resistance and longer service life. In contrast to metallic bearings, the tribo-polymers from igus do not require additional lubrication, […]

Read more...

Polymer bearings in adjustable seat posts

Alexander Muzicenko | 5. June 2020

The adjustable seat post is another variation of the seat post and is also called Dropper Post or Vario. This type is mainly used in mountain biking and has the advantage of height adjustment, which can be operated by remote levers. For downhill riding, the support can be lowered and raised for uphill or normal […]

Read more...

Polymer bearings in spring-mounted seat posts

Alexander Muzicenko | 5. June 2020

The seat post is an important component of a bicycle, especially when it comes to comfort. Not all roads are level and every impact is passed on to the rider. The saddle alone cannot absorb all impacts. The loads without suspension can have serious consequences for the back, for example. Essentially it is about more […]

Read more...

Advantages of polymer bearings in the bicycle

Alexander Muzicenko | 8. May 2020

In the bicycle industry, innovative solutions are not only focused on design, but also on the choice of materials. For example, for the frame there are many solutions made of aluminium or glass fibre reinforced material. Component manufacturers are also working flat out on the use of alternative materials. Be it saddle post, suspension, pedals […]

Read more...

Plain bearings for bicycle pedals – the advantages of polymer

Alexander Muzicenko | 24. April 2020

The bicycle is still very popular as a means of transportation. But whether the bike in question is a lifestyle product or a racing machine, the quality challenges for each component are great. Many technical components have profound effects on quality. There are shock absorbers and gear and brake components, of course, but bicycle pedals […]

Read more...