All messages - igus Blog - Page 220 All messages - igus Blog - Page 220

Feedthrough of draw wires

Martin Raak | 27. February 2012

For the series connection of joints, the 4 draw wires of the second (or upper) joint should be conducted through the first (or lower) joint. This feedthrough must be done in such a way that a movement of the lower joint does not alter the wire lengths of the feedthrough, which means Bowden cables are […]

Read more...

igus® robolink® with pneumatic gripper

Martin Raak | 7. February 2012

We build demonstration plants time and again for our own trade shows and of course for our igus® subsidiaries all over the world. Such systems are then shown, for example at the Hannover Messe or Motek, as well as in many smaller or the so-called house shows of customers.For some time we’ve been equipping our […]

Read more...

Tensile strength test report of robolink® wires

Martin Raak | 26. January 2012

robolink® wires were tested for tensile strength on the ZWICK tractor (nominal tensile strength > 3600 N).The nipple connection was fixed with different adhesives (see installation instructions for the wires). The experiments were carried out at room temperature and at 80°C.          Wire with brass nipples  Section of the mounted nipple Test […]

Read more...

igus® 4 DOF arm with drive unit in use

Martin Raak | 9. January 2012

Polytechnico di Torino in Italy uses a robolink® 4-axis arm with drive unit and angle sensors. Movement with voice control Vote Up +0 Vote Down -0You already voted!

Read more...

What options are available in triflex® R and what are the advantages of each?

Armin Gellweiler | 5. January 2012

    TRC versionThe TRC version has an enclosed design – cables and hoses are protected from damage through external factors such as chips or welding spatter. The following sizes are available: TRC.30.050.0TRC.40.058.0TRC.60.087.0TRC.70.110.0TRC.85.135.0TRC.100.145.0TRC.125.182.0 (*)   TRE versionThe TRE version has an “open design” with the igus® easy chain® system. Cables and hoses can be later […]

Read more...