Contaminated lubricant is one of the main causes of bearing damage and often a major factor in the premature end in the service life of bearings. Around 70% of bearing failures are caused by lubricant problems, such as contamination in the lubricant (25%), incorrect lubricant (20%) or too little lubricant (14%).
Due to the current situation with the Covid-19 virus, protective masks are our daily companion, whether in the supermarket or when visiting the doctor. Whether self-sewn or produced masks, almost everyone has at least one mask for their own needs. But what can you do if you have forgotten the mask and still have to […]
How does the production of a lead screw work? And what is the difference between the thread rolling and thread whirling manufacturing processes? To find out, we should first compare the two manufacturing methods of thread rolling and thread whirling.
The seat post is an important component of a bicycle, especially when it comes to comfort. Not all roads are level and every impact is passed on to the rider. The saddle alone cannot absorb all impacts. The loads without suspension can have serious consequences for the back, for example. Essentially it is about more […]
The adjustable seat post is another variation of the seat post and is also called Dropper Post or Vario. This type is mainly used in mountain biking and has the advantage of height adjustment, which can be operated by remote levers. For downhill riding, the support can be lowered and raised for uphill or normal […]