What is meant by the stick-slip effect? - igus Blog

What is meant by the stick-slip effect?

Lars Butenschön | 2. July 2019

What is meant by the stick-slip effect?

You are here:

The stick-slip effect refers to the jerking motion that occur when two solid bodies slide against each other. This phenomenon occurs when a body is moved whose static friction is significantly greater than the sliding friction. _x000D__x000D_
 
Imagine a heavy carton that you want to push over a smooth floor. The carton is heavy, which is why we have to use great force to overcome the static friction – that is, to move the resistance of the carton. The carton slides. Due to the smooth surface and the resulting low sliding friction, the carton is rapidly faster. However, the carton’s rapid sliding motion allows us to transfer less force to the carton. Finally, the force acting on the carton is no longer sufficient to overcome its static friction. The carton comes to a standstill, which requires us to apply much force again to overcome it and the process repeats itself. Adherence – releasing – sliding – braking – adherence – releasing … in reality, this effect is much faster and manifests itself in a stutter. . _x000D__x000D_
 
This phenomenon can be seen in a wide variety of areas. Wipers stutter over the windscreen of a car. When writing on the blackboard, chalk squeaks if you keep it at the wrong angle. Door hinges squeak. And stringed instruments such as the violin or the cello would not work, because their sounds arise by vibrations caused by stick-slip effect and vibration between the strings and the chords of the bows. _x000D__x000D_
 
For tribologically optimised materials, however, this effect is undesirable. The vibrations caused are transmitted to the overall structure and cause noises, which are often perceived as annoying squeaking or creaking. The desired sliding movement becomes an irregular stuttering and increases the wear of the bearings. These effects can be counteracted by minimising the difference between sliding and static friction, by using vibration dampening materials, by improving the rigidity of the overall structure (see pre-loaded bearings) or by separating the involved friction partners (for example by lubrication).

1. Force > static friction
The force (arrow 1) overcomes the static friction (arrow 2). The carton starts to move. _x000D_

2. Force = static friction
The static friction becomes sliding friction (arrow 2) and the carton slides quickly.

3. Force < sliding friction
The force (arrow 1) is not enough to overcome the sliding friction (arrow 2).

4. Force < static friction
The sliding friction becomes static friction. The force is not enough, the carton stops.

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Plain bearings

Newsletter:

Choose a topic now