robolink double articulated arm – speed test
Martin Raak | 23. September 2011
The high speeds of the robolink joint are tested with this testing system. The four degrees of freedom of the double joint are accelerated to an angular velocity of 150°/s. The average speed of the mounted weight (560 g) is thereby 1.05 m/s.
You are also welcome to comment on the article - we look forward to your opinion!