autoglide 5: Small lane, big effect! - igus Blog autoglide 5: Small lane, big effect! - igus Blog

autoglide 5: Small lane, big effect!

Christian Strauch | 18. February 2022

Why is the autoglide 5 so interesting, especially for short to medium lanes?

Explaining this requires some maths:

Example:

A travel distance of 50 metres with a busbar system compared to 50 metres with the autoglide 5:

Busbar system:

What is needed?

The busbar system itself:                           about 50 euros/metre = 2500 euros!

Optical data transmission:                     about 700 euros

Pantographs:                                        about 300 euros

Busbar system installation:                            three metres per hour; hourly wage: 40 euros/hour = 650 euros

Total: about 4150 euros

autoglide 5:  

  1. Harnessed energy chains including cables and data cable: about 70 euros/metre
  2. Assembly:   about three hours (for inexperienced personnel):  about 150 euros!

Total: 3650 euros

Conclusion: Energy chain is cheaper

This is a simplified example calculation without any claim to absolute accuracy, so a reader may remark, “He’s been awful generous with his estimates.”

But I really have not. The thing is, optical data transmission, which is quite expensive, has a high per-metre fixed cost component for small and medium lanes. The autoglide 5 uses a bus cable, which is included in the per-metre calculation and is inherently much cheaper than an optical data transmission system.

So the shorter the lane, the more most cost-effective it is to use the autoglide 5 instead of a busbar system. The break-even point is somewhere beyond 80 metres.  It is impossible to say exactly where it is because every producer has different purchasing conditions – there are busbar system manufacturers and data light barrier manufacturers.

For short and medium lanes, the autoglide 5 is without rival!

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!