The energy chain in the lane – Part 3
Christian Strauch | 18. March 2020
autoglide 5: Scope of delivery
The autoglide 5 is a brand new product from igus. It is unclear to what extent the chain is offered. But at the moment we are working on being able to offer the complete package. That means:
- The autoglide 5 as such: Energy chain type 2400.07.075.0 with autoglide crossbars on the inner radius and special crossbars (with the groove) on the outer radius.
- The appropriate cables, i.e. motor cables as single cores and a data cable, i.e. bus or fibre optic cable. Optionally harnessed with connectors or wire end sleeves or other connectors.
- The steel cable, already designed for your travel length and provided with an “eye” at both ends.
- Dowel and screw anchor for connecting the steel cable

First of all, this is the standard we follow at igus. Changes can still be made and, of course, the customer can also procure the components, in addition to the energy chain, on his own responsibility if expressly requested. However, this should then be done in consultation and technical clarification with igus to ensure the function of the autoglide.
You are also welcome to comment on the article - we look forward to your opinion!