The maximum tensile strain of a cable? - igus Blog The maximum tensile strain of a cable? - igus Blog

The maximum tensile strain of a cable?

Jan Arnoldy | 5. May 2020

The maximum tensile strain of a cable is particularly important where cables are used in hanging applications. Because there the cable must carry its own weight. This is the case in the lifting movement of a storage and retrieval unit (SRU).

Storage and retrieval unit maximum tensile strain

The maximum tensile force for cables

The maximum tensile strain indicates up to which force or up to which freely suspended length a cable can be loaded without danger. Depending on the cable structure, there can be quite different maximum tensile strains, since the tensile strain is always calculated according to the sum of the cross sections of all the main cores of a cable. The maximum tensile force for cables with copper cores is specified in VDE0298. This defines the maximum permissible tensile force for standard cables with 15N/mm² cross section of the sum of the main cores.

A calculation example can clarify the facts of the case:

Assuming a CF21.25.15.02.02.UL, i.e. a servo cable with a structure of (4G2.5+(2×1.5)C)C, should be used in a hanging application of 25m. First the weight of the cable must be calculated:

F=m x a x l = 0.271kg/m x 9.81N x 25m = 66.5N

How high a load can be applied on the cable? The main cores therefore have a cross section of 2.5mm²:

4G2.5mm²          -> 4×2.5mm²=10mm²

10mm² x 15N/mm² = 150N max. permissible tensile strain

Since the weight of 66.5N is less than the maximum permissible tensile strain of 150N, the cable can be used in this application.

Which cable should be used for high tensile strains?

Especially with small cross sections such asbus cables, the permissible limit is quickly reached, which is why igus offers the optimum cables especially for applications with very high tensile strains. A good example of such a cable is the CFSPECIAL182.045. This is a CAT5e Ethernet cable. Due to its special structure with an aramid braiding in a two-layer outer jacket, this cable is highly suitable for applications with very high tensile strain, such as in hanging applications.

CFSPECIAL.182.045

The aramid braiding integrated in the outer jacket ensures that the tensile strain does not act on the inside of the cable, but is absorbed in the braiding. This ensures a longer durability and the smooth function of the cable.

Insanely high tensile forces also occur in other applications, e.g. in forklifts.

It is necessary to take a closer look and examine the details in order to find a good solution, as the form of movement in this application is also different, as the cable is guided via rollers.

Maximum tensile strain with the example of a forklift

Conclusion

The maximum tensile strain is extremely important when selecting the right cable. If you do not pay attention to it, the cable used may “lengthen”. This can lead to defects and in the worst case to machine failure.

Do you need help with your application? We are here for you and are happy to advise you.

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!