Sintered bushings or plain bearings made of sintered bronze are used in many bearing applications. They are comparatively cheap to procure, available in many dimensions and are sold as “self-lubricating” or “maintenance-free”. However, sintered bushings are by no means as universally applicable as many users think. In this blog post, I will take a closer […]
Many plant operators know the problem: when installing metal ball bearings, lubrication is essential. This procedure has to be repeated at regular maintenance intervals and that not only swallows up money, but also a lot of time. As a ball bearing alternative, xiros is well suited.
I am asked time and again what igus has to do with cables? After first cringing at my self-conception, I relax and am happy to be able to answer this question. I’ll start at the beginning: my heart beats for electrical engineering and before I came to igus, I knew cable only as a connector […]
The current weather situation is impressive. Temperatures in Germany go below -25 degrees at night. I haven’t experienced that very often. There are beautiful natural spectacles from huge icicles to frozen waterfalls. Besides these beautiful perspectives, however, there are also less beautiful ones. Roads freeze over, rail traffic comes to a standstill. Some machines freeze […]
The defect of a ball bearing can have various causes; whether cage wear, ball breakage or damage to the running surfaces. Find out in this blog post why igus can be an alternative to metal after a defect.