November, 2020 - igus Blog - Page 3 November, 2020 - igus Blog - Page 3

Which ball bearing seals are available and why doesn’t igus need additional markings

Patrick Czaja | 13. November 2020

Many metallic rolling bearings are available as a sealed version Ball bearing seals are usually mandatory for the metallic version, otherwise dirt will get into the running surfaces of the ball. They can combine with the lubricant and block the bearing run. Ball bearings made of polymer or ceramic are mostly only available as an open type. Why? Find out here.

Read more...

How do I find out the DIN installation size of the metal ball bearing? And how do I find the igus® counterpart?

Patrick Czaja | 11. November 2020

For metallic ball bearings, determining the installation size is usually simple. Usually the type designation is printed either on the inner or outer ring. It becomes more difficult, however, if the imprint remains unrecognisable despite cleaning. Therefore the ball bearing must be measured manually at this point. _x000D_   I now know my ball bearing […]

Read more...

Where are cables used?
chainflex cables in stage technology

Sascha Mais | 11. November 2020

Sometimes, our business actually resembles show business. So we can identify wonderfully with the slogan “The show must go on”. And in the events industry this is probably also true. Failures cannot be afforded here. It must go on forever. How cables in stage technology contribute to success is the subject of today’s article. Stage […]

Read more...

Despite the harsh environment: this energy chain operated for 18 years

pwirth | 9. November 2020

We are not surprised, but nevertheless excited about the news from a customer in the pipe manufacturing industry: for 18 years a first generation rol e-chain has been providing reliable service there –  in harsh environments. Newer systems will surpass this record. What happens in 18 years?: a child is born, learns to walk, graduates […]

Read more...

Is it ok if the spherical ball rotates inside the spherical bearing housing?

Peter Hughes | 6. November 2020

This is a question we hear a lot when customers ask about igubal® spherical bearings. Customers often wonder if this is acceptable and if it has any effect on their application. I’d love to give here a short answer like “Yes” or “No”. But in fact, it depends on the type of igubal bearing and […]

Read more...