If one takes a look at the chainflex catalogue, one quickly realises that igus has many different cable types of the same kind in its range. In the section on control cables alone there are 19 different cable ranges. Why is that? The range of control cables includes cables with overall shield as well as […]
When threads are used in heavy-duty applications, they must meet many requirements. One of the most important aspects for heavy loads is the stability of the threads under high axial and radial loads. But does this also work with lead screw nuts made of polymer? Clear answer: Yes! The drylin lead screw technology development team has set itself the task of developing a robust alternative to the flange lead screw nut.
There must be an answer to this question. After all, there are a limited number of “best Italian restaurants”, “best frozen pizzas” and “best TV series”. And we haven’t even got to narrowing it down. The best Italian restaurant in Bonn? Or in the whole world? The question of the best plain bearing for farm machines is like that.