Where are stainless steel linear modules used, and what advantages does stainless steel have over other materials such as aluminium?
Cables are used in many areas. Some cables must meet very special requirements or withstand certain external factors. Consider cables that are used under water. What problems arise for cables used in underwater applications? What solution approaches are there? Longitudinal and transverse waterproofness There are a number of things that cables that are used under […]
The two most common reasons for manufacturing drive and lead screw nuts using 3D printing processes are the construction of functional prototypes and the production of complex custom nuts. In product development, several models are sometimes designed and tested – with the rapid prototyping process, the production of near-series variants and customisations can be carried […]
How does a 50-year-old energy chain fit into Industry 4.0, the future-oriented project of comprehensively digitalising industrial production? To hold your own in international business competition, it is necessary to be intimately familiar with what your customers want. Technologies Production for individual customers at low prices with short delivery times can often be achieved only […]
Normally, plain bearings are intended for installation in relatively thick-walled designs. The plain bearing is pressed into a hole of recommended tolerance, where it remains. Press-fit can be difficult if the components have thin walls. But beyond fixing in place, there are other pitfalls which we will examine more closely here. Then I will give […]