Ball bearings consist of an inner and outer ring, a cage and rolling elements. The cage is used to separate the rolling elements from each other in the form of balls. If the balls were not separated, they would run against each other and overheat. With high rotational speeds and friction of the balls, destructive […]
This abbreviation stands for Control and Communications Link. It is a fieldbus system developed by Mitsubishi in 1996. This bus system is mainly used by automation systems made in Asia. Due to strong customer demand, CC-Link was launched in the market in 1999 as an open network. Third-party providers were also able to develop interfaces […]
Machine tools have become an integral part of the industry. Thanks to them, metallic workpieces are produced with the highest precision, which are used, for example, in the automotive industry or in the aerospace industry. In all machine tools the desired contour is achieved by the interaction of tool and workpiece. Depending on the technology, […]
Wherever there is food contact, cleaning must be frequent and intensive. It is the same in the food processing industry and it is also the same in the manufacture of vending machines. There are strict rules for this, resulting from the regulations of the European Parliament.
In the case of indoor cranes, the main power supply is usually provided via busbar systems and data transmission via wireless data systems. A drum solution (motor-driven or spring balancer) is generally used for large or harbour crane systems. Information about the drum solution can be found in the article with the title: Harbour / Large Crane Main Power and Data Supply.