xiros® plastic ball bearing
Our ball transfer units can be used to move fragile or heavy goods easily and in all directions without much effort. We use various design concepts for this. In addition to injection-moulded housings with housing pads and ball beds, we also offer a variant with a sliding insert specially designed for higher loads and shock […]
Hardly any industry can do without electric motors in the entire value-added process and the demands placed on products are constantly increasing. Similarly, the requirements for the various components of the drives are also increasing in order to ensure smooth production processes, including for the bearing of components, namely ball bearings for electric motors. But […]
Deep groove ball bearings according to DIN 625 standard are the most commonly used ball bearings in industry. Depending on the application, plant operators have different requirements for the installed machine components. For deep groove ball bearings, for example, the possible speeds per minute are usually important. Which ball bearing is suitable for high speeds? And that even made of plastic? xiros is the answer.