Wear
The number of plain bearing solutions is virtually infinite, and there are no fewer designs of suitable – and unsuitable – shaft materials. In fact, different shaft materials and their coatings can create completely different wear patterns for the same plain bearing. This blog entry will deal with two frequently used shaft coatings and consider […]
3D printing is ascendant across industries and materials, not only in product development, but also in industrial manufacturing processes. But if the freedom granted by additive manufacturing is to realise its full potential in the industrial environment, 3D printing materials must perform just as well as their mechanically processed counterparts. igus has dedicated itself to […]
Only one short work step left … and then it happens. The device refuses to work. The knee lever seizes, and the machine performs an emergency stop. The user has just one concern: “How long does the service technician need?” “Why can’t this piece of junk keep it together until I’m done with this urgent […]
And again the working platform cracks, squeaks and crunches when the hydraulics are actuated. If noise is generated during operation or the device even jams, it is often already too late. Once you (or the appointed service technician) have located and dismantled the bearing, it often flashes and shines at you. Something like that! A […]