STEP data
I want to supply more data for you to be downloaded, especially about our RL-DC “standard arms”. Our standard arms include all joints, motors, connections (=c-shaped metal sheets), cables and chains. Attached our NEW catalogue (now also available in ENG), STEP data for our 8 standard configurations and also the related drawings with part lists. […]
At the HMI trade show we released our strain wave gear (RL-S) as a product in addition to our worm gears (RL-D). The smallest version of the strain wave gear (RL-S-17-N11-00-28-020K0) is used for the fifth axis in the standard joint arms RL-D-RBT-5532S-XX and RL-D-RBT-3322S-XX. The RL-S-17 gear comes in two variations, both have a […]
We have been involved in the development of a new open source teen size soccer robot for 2 years now (and theĀ improvement still goes on!). The main development was done by the University of Bonn, institute AIS, Professor Sven Behnke, who also developped our open source robolink software IME (igus motion editor), igus contrubuted the […]
since October 2015, the standard version of RL-D-50 (-101 and -102) is also available from stock. The missing PRT-02-50 version was the reason for the delay. Please find attached here the STEP data for our joints for all variants and sizes, as well as for a collection of motor kits (with igus stepper motors). These STEP […]
The Basic idea of our NEW RL-D Joints is, that every Joint can be composed out of several components (Joint kit). Main differentiations are: # Rotary sliding bearing igus PRT-01 (aluminum table with iglidur J sliding elements) or PRT-02-AL (aluminum ring with compact plastic ring made of iglidur J4) or PRT-02-LC (outer aluminum ring replaced […]