Long travel
About a year ago, we introduced the autoglide 5. Unlike its “mother”, the autoglide 5, which is based on our “2400” energy chain, does not need a guide trough on long travels, even with the highest dynamics and travels of up to 80 metres. Also see older blogs! The puzzle behind this very innovative product […]
A gliding application frequently looks better than an unsupported energy chain. This is not just because the straight line of the upper run, but also because the sag leading to the chain drop is eliminated. This allows unsupported systems to better use the space at the end of the travel. But at high fill weights […]
The E4/4 rol e-chain is familiar from the crane industry among others. But what does this have to do with the machine tool? High loads, long travels and a dynamic behaviour, this description also frequently applies to x-axes in machine tools. The rol e-chain 5050RHD, for example, allows travels of 10-800m with a maximum fill […]