light
Widespread in the animal kingdom, for people an option. The skeleton on the outside of arthropods provides stability in the same way as the endoskeletons of mammals. Why not combine the advantages of the two systems with each other? An endoskeleton (inside the body) is strong but, having numerous joints, is nevertheless very flexible. It […]
A stage setting like this in a theatre or opera house is an impressive view every time you see it. There are a lot of lights and hidden technology, which require a certain degree of cable management to achieve. As it is with most stages, the available space which can be used to guide and […]