Laboratory tests
Producing energy from renewable sources is always associated with high costs and investment. Various factors such as procurement, financing and operating costs play a significant role. An important consideration is the system’s service life – a long one means that these costs can be recouped over a longer period. Photovoltaic systems, especially solar modules, nowadays […]
The adjustable seat post is another variation of the seat post and is also called Dropper Post or Vario. This type is mainly used in mountain biking and has the advantage of height adjustment, which can be operated by remote levers. For downhill riding, the support can be lowered and raised for uphill or normal […]
igus has the world’s largest test laboratory for plastics in moving applications in Cologne, with around 12,000 tests per year. This includes tests that demand everything from the most diverse materials under the most adverse conditions. At the present test, a xiros fixed flange ball bearing competes against its metallic counterpart in a salt water […]