IF – igus Blog

Keyword:

IF

Which ball bearing is suitable for high speeds?

Patrick Czaja | 2. June 2022

Deep groove ball bearings according to DIN 625 standard are the most commonly used ball bearings in industry. Depending on the application, plant operators have different requirements for the installed machine components. For deep groove ball bearings, for example, the possible speeds per minute are usually important. Which ball bearing is suitable for high speeds? And that even made of plastic? xiros is the answer.

Read more...