Gantry
Machine tool cycle times are being continuously optimised, and loading and unloading must therefore be correspondingly quick. When the gantry is larger, it is especially important that the energy supply keep pace. For travels of 10m or more, the P4 series is well ahead of the pack. This chain is the latest generation of igus […]
A gliding application frequently looks better than an unsupported energy chain. This is not just because the straight line of the upper run, but also because the sag leading to the chain drop is eliminated. This allows unsupported systems to better use the space at the end of the travel. But at high fill weights […]