Filling
Since food and beverages are sensitive products, production and processing must also be precisely tailored to them. This applies in particular to direct food contact. For this reason, there are igus materials that have been specifically developed for the requirements of the food and beverage industry. Starting with FDA-compliant, later EU 10/2011-compliant materials were added. […]
When a new product is being developed or shortly before a food, packaging, or beverage machine test phase, receiving prototype samples of a plain bearing or other components as quickly as possible can be very important. iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is […]
igus has many different linear guides in its product range. For example, drylin W offers a large modular system. drylin N is the first choice for extremely low-profile installation heights. drylin T is identical in construction to the usual recirculating ball bearing guides. A representative of the shaft guides is drylin R. Since some machine […]
Many different machines are used in the packaging, food, and beverage industries. There is one thing that most of the different machine types have in common though: they are regularly and intensively cleaned. And they are cleaned at temperatures often above 100°C. igus offers several polymer plain bearings that have no problem at these high […]