e-bike
The adjustable seat post is another variation of the seat post and is also called Dropper Post or Vario. This type is mainly used in mountain biking and has the advantage of height adjustment, which can be operated by remote levers. For downhill riding, the support can be lowered and raised for uphill or normal […]
The seat post is an important component of a bicycle, especially when it comes to comfort. Not all roads are level and every impact is passed on to the rider. The saddle alone cannot absorb all impacts. The loads without suspension can have serious consequences for the back, for example. Essentially it is about more […]
The bicycle is still very popular as a means of transportation. But whether the bike in question is a lifestyle product or a racing machine, the quality challenges for each component are great. Many technical components have profound effects on quality. There are shock absorbers and gear and brake components, of course, but bicycle pedals […]
In the last few years, the bicycle has changed from a mere object of utility to a weight-optimized lifestyle object. Not least the electrification has contributed significantly to this trend. Customers want as quiet a run as possible. The excessive background noise of the bicycle chain on the e-bike is a thorn in the side […]