drylin R
Whether in a welded construction of a road/rail vehicle, or in the interior of a double-decker train; you have to work with tolerances everywhere and be able to compensate for them. Especially when linear, pivoting or rotary movements should continue to function without problems.
igus has many different linear guides in its product range. For example, drylin W offers a large modular system. drylin N is the first choice for extremely low-profile installation heights. drylin T is identical in construction to the usual recirculating ball bearing guides. A representative of the shaft guides is drylin R. Since some machine […]
Wherever food or beverages are processed, filled or packed, contamination can occur. If it is salt or sugar, it is important to take a close look at the abrasive (rubbing/grinding) wear. In this way it can be determined what influence this has on the plain bearing or linear guide. In order to examine such contamination, […]