Drive technology
Linear axes and linear modules can be driven differently. Which system is the right one for me – lead screw drive or toothed belt drive?
Where are stainless steel linear modules used, and what advantages does stainless steel have over other materials such as aluminium?
Today’s high-frequency-controlled drives and motors, so-called Variable Frequency Drives (VFD), are demanding and technically sensitive. The servo cables used for this purpose are therefore not only means to an end, but ultimately even tip the scale. Why? Because even the nature of the materials used, in this case, the insulation material, can have a huge […]