Current carrying capacity
The current carrying capacity of cables is one of the decisive selection parameters, especially in the field of energy transmission, or for classic motor and servo cables. The DIN VDE 0298-4 says amongst other things:“The current carrying capacity is the maximum permissible current under certain conditions at which the conductor is not heated above the permissible […]