Coating
Powder lacquering, also known as powder coating, can be easily applied to conductive materials by means of electrostatic charging. For this purpose, the component is charged and the powder is applied using a spray gun in the tribo or corona charging process. The powder adheres to the component and thus builds up a uniform layer. […]
Surface coatings have long since established themselves in all areas of everyday life. From frying pans to bicycle frames, the range of different coating materials and their properties is huge. A more recent phenomenon is the so-called tribological polymer coating. These are plastic-based coatings that have been additionally improved tribologically – i.e. for use as […]
Often enough, it is the surrounding factors such as housing hole, shaft and other elements that predetermine what plain bearing dimensions are chosen. Then whether a bearing with a length of 10mm or 12mm is selected only depends on the price or availability. But what about when these factors delimit the choice so tightly that […]