…my sensor need? (Number of cores, cross section of cores) What connector combination should the cable have to connect sensor and control unit? (M5, M8, M12, 7/8″, 1/2″ straight, angled,…
…design process?
But where do they start in the design process? In most cases, the individual components such as the necessary sensor technology for plant monitoring or the software
…
…to be optimised by means of smart maintenance. These can be critical, particularly expensive or even simple systems (parts) that are already equipped with the required sensor technology. Caution is…
…thanks to the integrated sensor technology. This is done by continuously measuring the electrical resistance in the sensor material. If this resistance changes, the sensors indicate that the component must…
…sensor Temperature sensor GPS sensor Kitchen personal weighing scales
I hope the kitchen scale with its sensors also passed off as a positive association. It is also noticeable that
…