Low Cost Automation
The robolink highlights at the Hannover Messe 2010 – round tour through the stand and presentation of novelties. Vote Up +0 Vote Down -0You already voted!
Increase in the transmitted torque (rotation) from 5 (generation 1) to 7 Nm (generation 2) in continuous operation. (Damage in the one-off fracture test at > 24 Nm) GFRP and CFRP rods now available in profiled version. Maximum length of 1 m. See price list. Weight CFK: 170 g/m, GFK: 200 g/m, Aluminum 270 g/m […]
Our beta tester special offer has been running since the end of December. So far approx. 30 customers have been sent samples and approx. 20 customer-specific tests are running. More samples are being produced to keep up with the demand. Applications areas / industries: research centers (Fraunhofer, DLR, international universities), robot builders (service, maintenance, handling), […]
The revised, new version of the articulated robot joint is now available as a prototype. The following product improvements have been achieved: lower cable friction due to less narrow cable guide for the rotational motion (newly laid Bowden cables with optimized friction couple => see figures) New design of the transition from articulated joint to […]
We originally wanted to manufacture injection molded tools in connection with the HMI in order to produce the product as shown.Increase the transferable torques by means of design improvement to the transfer between articulated joint and rod, reduce cable friction by making changes to the design and materials, but above all: integrate magnetic sensors to […]