…then transferring the solder blister to the soldered joint does not produce a reasonable result. As the solder joint is cold, the solder cannot form a connection with the component.
…
…a suitable workplace, the choice of solder and flux is another important factor:
Lead-free solder has the advantage that in addition to the main component tin (Sn – 90…
…feature of this soldering method. Solder joints wetted with solder are heated up to soldering temperature in a precisely defined temperature-time profile of the assembly. This method includes the heating…
…the components. After heating the solder, the electricity supply is terminated. The solder fills small gaps, levels uneven places and finally solidifies.
Resistance soldering is usually used for hard…
Flame soldering is a thermal joining process for metallic materials that are connected with a solder during this method. The thermal energy required for this procedure
…